Solution
This manual applies to UFC200 chargers that has AC Plug
In order to successfully replace the control boards, steps bellow have to be followed:
1. Turn off charger with RCBO1 + Pull out the main fuses from the input.
Figure 1. RCBO1 and main fuses
2
2. Locate the control boards that needs to be replaced.
Figure 2. Main Board, Display Board, DC control boards
3. In order to replace Main and Display board, protection plate with a Fan needs to be removed. Loose 4 nuts and lift up the plate.
Figure 3. Protection plate with a fan
4. Start replacement of the control boards for those that were provided by Delta – DO NOT MIX THEMwith original ones from charger.
5. Once the control boards are replaced, reworked cable have to be installed in between Main and Display Board
Figure 4. Reworked cable that needs to be installed in between Main Board and Display Board
6. Remove SIM Card and SD card from original Main Board and Display Board and insert it into the newly installed one – do NOT mixed them up in between each other.
Figure 5. SD cards in Main board and Display board
8. Make sure that all replaced control boards have a white sticker.
Please note that the Display Board has 1 RED sticker from rework v3
Figure 7. Detail of Main board and DC board with white stickers
9. Insert back main fuses into the Input terminal block and turn on charger with RCBO1.
10. Contact L2 Delta Engineer to generate a new License Key for charger.
IMPORTANT Note
In case that the following communication cable is present in the charger, it must be replaced for the original non-reworked version
Figure 8. Reworked version which must be replaced for original
By using Delta Electronics (Netherlands) B.V. and affiliates website and its technical information, you agree to be bound by the terms of this warranty disclaimer.