Solution
This manual applies to UFC200 chargers that only Double DC or DC + AC Socket.
In order to successfully replace the control boards, steps below have to be followed:
1. Turn off charger with RCBO1 + Pull out the main fuses from the input.
Figure 1. RCBO1 and main fuses
2
2. Locate the control boards that needs to be replaced.
Figure 2. Main Board and DC control boards
3. In order to replace Main board, protection plate with a Fan needs to be removed. Loose 4 nuts and lift up the plate.
Figure 3. Protection plate with a fan
4. Start replacement of the control boards for those that were provided by Delta – DO NOT MIX THEMwith original ones from charger.
5. Remove SIM Card and SD card from original Main Board and insert it into the newly installed Main board.
Figure 4. SD cards in Main board
6. Make sure that all replaced control boards have a white stickers.
Figure 5. Detail of Main board and DC board with white stickers
7. Once the control boards are replaced, following cable have to be disconnected and removed
Figure 6. Flat cable between Main board and Display board has to be removed
In case that the following communication cable is present in the charger, it must be replaced for the original non-reworked version
Figure 7. Reworked version which must be replaced for original
By using Delta Electronics (Netherlands) B.V. and affiliates website and its technical information, you agree to be bound by the terms of this warranty disclaimer.